Analog Devices' AD8233 AFE for Medical Wearables Now Shipping from Mouser
November 28, 2016 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the AD8233 analog front end (AFE) for heart monitor devices from Analog Devices. The AD8233 AFE is a fully integrated, single-lead electrocardiogram (ECG) front end designed in a compact, easy-to-use component. The low-power biopotential AFE enables smaller, lighter, and less obtrusive cardiac monitoring devices with longer battery life. The highly integrated AD8233 AFE eliminates unnecessary costs and extra design time, helping developers get products to market more quickly.
The Analog Devices AD8233 analog front end, available from Mouser Electronics, is an integrated signal conditioning block designed to extract, amplify, and filter small biopotential signals in the presence of noisy conditions, such as those created by motion or remote electrode placement. This design allows for an ultra-low-power analog-to-digital converter (ADC) or an embedded microcontroller to easily acquire the output signal.
The device's tiny, 2.0mm × 1.7mm footprint enables designers to create wearable health devices that are smaller, lighter, and easier to wear. Along with its small size, the single-supply (1.7V to 3.5V) AD8233 features extremely low quiescent current of 50 μA (typical), resulting in greatly extended battery life that helps support continuous monitoring without the interruption of a recharge or battery replacement.
For ease-of-use and flexibility, the AD8233 includes an integrated right leg drive (RLD) amplifier with shutdown plus an uncommitted op amp. The device also provides a two-pole adjustable high-pass filter, a three-pole adjustable low-pass filter with adjustable gain, and a radio frequency interference (RFI) filter to allow for consistent, confident operation in an inherently harsh electrical environment under a range of use cases. The AD8233 is supported by the AD8233CB-EBZ evaluation board, a ready-to-use AFE tool with the necessary inputs, outputs, supplies, and leads routed to test pins to simplify connectivity.
To learn more, visit http://www.mouser.com/new/Analog-Devices/adi-ad8232-amplifier/.
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 22 global support locations and stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 600 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Analog Devices Inc.
Analog Devices has built one of the longest standing, highest growth companies within the technology sector utilizing cultural pillars such as innovation, performance, and excellence. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 100,000 customers, representing virtually all types of electronic equipment. Celebrating over 50 years as a leading global manufacturer of high-performance integrated circuits used in analog and digital signal processing applications, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices' is included in the S&P 500 Index. For more information, visit http://www.analog.com/.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com