Mouser Now Stocking New TDK AMT45S Pulse Transformer for Automotive EV Charging Applications

For Immediate Release

Connect With Us


Learn more about the AMT45S pulse transformer
Learn more about the AMT45S pulse transformer

June 4, 2026Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new AMT45S pulse transformer from TDK. The AMT45S is designed for power line communication (PLC) circuits in EV charging applications.

The TDK AMT45S pulse transformer, available from Mouser, is designed to comply with the European CCS (Combined Charging System) and US NACS (North American Charging Standard) standards for rapid expansion of charging infrastructure. These standards rely on PLC for charging control, and the performance of the pulse transformer is directly linked to the reliability of overall charging efficiency, charging control communication, and battery performance.

The AMT45S pulse transformer is manufactured using fully automated winding technology. This proprietary process features metal terminals and laser welding to offer low insertion loss and high reliability across the 2 MHz to 30 MHz frequency band.

By facilitating miniaturization, the AMT45S ferrite and winding geometry, and the lack of a resin coating also provide higher production efficiency, improved quality stability, and greater cost-effectiveness than traditional products. The AMT45S features a compact 4.7 × 3.4 × 3 mm3 (L x W x H) footprint and an operating temperature range of -40°C to +125°C.

To learn more, visit https://www.mouser.com/new/tdk/tdk-amt45s-pulse-transformers/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About TDK

2026 - TDK Corporation is a world leader in electronic solutions for the smart society based in Tokyo, Japan. Built on a foundation of material sciences mastery, TDK welcomes societal transformation by resolutely remaining at the forefront of technological evolution and deliberately "Attracting Tomorrow." It was established in 1935 to commercialise ferrite, a key material in electronic and magnetic products. TDK's comprehensive, innovation-driven portfolio features passive components such as ceramic, aluminium electrolytic and film capacitors, as well as magnetics, high-frequency, and piezo and protection devices. The product spectrum also includes sensors and sensor systems such as temperature and pressure, magnetic, and MEMS sensors. In addition, TDK provides power supplies and energy devices, magnetic heads and more. These products are marketed under the product brands TDK, EPCOS, InvenSense, Micronas, Tronics and TDK-Lambda. TDK focuses on demanding markets in automotive, industrial and consumer electronics, and information and communication technology. The company has a network of design and manufacturing locations and sales offices in Asia, Europe, and in North and South America. 

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764