Mouser Now Stocking New Sensirion SHT4xA Relative Humidity/Temperature Sensors for Automotive Applications

New Product Announcement

Connect With Us


September 6, 2023Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now shipping the  SHT4xA relative humidity/temperature sensors from Sensirion. The SHT4xA are 16-bit, high-accuracy, automotive-grade digital sensors for measuring relative humidity and temperature with different accuracy gradings, explicitly developed for the most demanding automotive reliability application requirements.

The Sensirion SHT4xA relative humidity/temperature sensors, available from Mouser, are designed for operation in harsh automotive environments, like accelerated lifetime tests at 85°C / 85 %RH. The SHT4xA sensors are AEC-Q100 rated and feature a powerful, integrated, on-chip heater with advanced onboard diagnostics for self-decontamination and periodic creep compensation in applications with prolonged high humidity. The SHT4xA sensors achieve accuracy tolerances of ±2 %RH and ±0.2°C from 0 %RH to 100 %RH at -40°C to +125°C, with operating voltage ranges of 2.3 V to 5.5 V.

Suitable for surface mount technology (SMT) processing, the SHT4xA sensors’ four-pin, dual-flat-no-leads package offers different accuracy classes, with I2C or pulse-width modulation interfaces, and with optional wettable flanks, enables automated optical inspection of the robust DFN package.

The SEK-SHT40A-AD1B temperature evaluation kit, also available from Mouser, is used to evaluate the SHT40A sensor. The kit includes three SHT40A sensors on an FPCB and a one-meter-long RJ45 adapter cable. The SEK-SHT40A-AD1B evaluation kit is designed to work with the Sensirion SEK-SensorBridge environmental sensing kit.

To learn more about the SHT4xA sensors, visit https://www.mouser.com/new/sensirion/sensirion-sht4xa-sensors/.

To learn more about the SEK-SHT40A-AD1B evaluation kit, visit https://www.mouser.com/new/sensirion/sensirion-sek-sht40a-ad1b-eval-kit/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Sensirion

2026 - Sensirion is a leading sensor manufacturer, providing relative humidity sensors and flow sensor solutions with unique performance. The company's product range includes liquid flow sensors, mass flow meters, mass flow controllers and differential pressure sensors. Using Sensirion's microsensor solutions, OEM customers benefit from the proven CMOSens® technology and excellent technical support. Among a large variety of applications, flow and humidity sensors are successfully used in the automotive and medical industries.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764