NXP’s LX2 QorIQ Layerscape Processors, Now Available at Mouser, Support the Next Generation of Innovative Networks

New Product Announcement

Connect With Us


NXP’s LX2 QorIQ Layerscape Processors, Now Available at Mouser, Support the Next Generation of Innov

May 13, 2021 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the QorIQ® LX2160A, LX2120A, and LX2080A (LX2) Layerscape® processors from NXP Semiconductors. Built on up to 16 Arm® Cortex®-A72 processor cores, the LX2 processors feature scalable data path acceleration logic, as well as the network and bus interfaces required to support applications including storage, networking, wireless infrastructure, military, aerospace, and telecommunications.

The NXP LX2 QorIQ Layerscape processors, available at Mouser, comprise the LX2160A, LX2120A, and LX2080A, which include 16, 12, and eight Arm Cortex-A72 processor cores, respectively, delivering high performance of up to 2.2 GHz. The processors are supported by a consistent API providing both simple and complex manipulation of the devices' hardware peripherals.

The processors feature 16 Mbytes cache, 2 Mbytes packet caching buffer, and a 122 Gbit/s Layer 2 Ethernet switch. The versatile processors offer up to 16 Ethernet ports, up to 24 PCIe Gen4 lanes, and 24 SerDes lanes operating up to 25 GHz.

For designs with size constraints, the LX2162A, LX2122A, and LX2082A processors offer the processing capabilities of the LX2xx0A devices in roughly a quarter of the size. Suitable for small boards such as network interface cards and custom daughter cards, the LX2xx2A processors integrate low-power 16nm FinFET process technology to support optimum performance in a limited form factor.

To learn more about the LX2160A, LX2120A, and LX2080A processors, visit https://www.mouser.com/new/nxp-semiconductors/nxp-lx2160a-lx2120a-lx2080a-processors/.

For more information on the LX2162A, LX2122A, and LX2082A processors, go to https://www.mouser.com/new/nxp-semiconductors/nxp-lx2162a-lx2082a-lx2122a-processors/.

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764