Now at Mouser: Lattice Semiconductor CertusPro-NX Versa Evaluation Board for Rapid Prototyping of FPGA Designs

New Product Announcement

Connect With Us


Learn more about the CertusPro-NX Versa evaluation board
Learn more about the CertusPro-NX Versa evaluation board

March 2, 2026Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the CertusPro™-NX Versa evaluation board from Lattice Semiconductor. Designers can use the CertusPro-NX Versa board to explore and experiment with the features of the CertusPro-NX Field-Programmable Gate Array (FPGA).

The Lattice Semiconductor CertusPro-NX Versa evaluation board, now at Mouser, allows engineers to rapidly prototype and test applications based on the CertusPro-NX FPGA. The evaluation board supports a 128-MB Serial Peripheral Interface (SPI) flash with a quad read feature. The board also features an on-board download controller for programming the CertusPro-NX FPGA device. The evaluation board can be used to expand CertusPro-NX FPGA usability with SFP, PCIe, and CSI interfaces, a MIPI CSI-2 camera connector, a USB3 Controller, Raspberry PI HAT, and Pmod connectors, with access to two SerDes channels. The CertusPro-NX Versa evaluation board kit includes a 12V adapter and international plug adapters, a USB cable for programming via PC, and a quick-start guide. Easy-to-use resources, such as jumpers, LED indicators, push buttons, and switches, are available for user-defined applications.

To learn more, visit https://www.mouser.com/new/lattice-semiconductor/lattice-certuspro-nx-versa-evaluation-board/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Lattice Semiconductor

2026 - Lattice Semiconductor is the low-power programmable leader, solving customer problems across the network, from the Edge to the Cloud, in the growing communications, computing, industrial, automotive, and consumer markets. Through differentiated low-power, small-sized programmable logic products and related solutions, long-standing relationships, and commitment to world-class support, Lattice enables its customers to quickly and easily unleash their innovation to create a smart, secure, and connected world. In addition to innovative FPGAs, Lattice provides customers with a comprehensive support ecosystem that includes powerful, easy-to-use design tools, IP cores, reference designs, development kits, and local technical support.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764