New at Mouser: Atmosic Technologies ATM34/e SoCs for Industrial, Smart, and Robotics Applications

New Product Announcement

Connect With Us


Learn more about the ATM34/e SoCs
Learn more about the ATM34/e SoCs

June 10, 2026Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the new ATM34/e system-on-chip (SoC) from Atmosic Technologies. The ATM34/e SoCs offer extremely low-power Bluetooth® 6.0 SoCs with an energy-harvesting option, designed to extend battery life for industrial IoT sensor devices found in asset tracking and tags, remote monitors, and security applications.

The Atmosic Technologies ATM34/e SoCs, available from Mouser, integrate Bluetooth 6.0-compliant radios with a 64 MHz Arm® Cortex® M33F application processor, RAM, ROM, NVM, Arm TrustZone® security, and state-of-the-art power management. They enable the efficient capture, use, and storage of energy from RF, heat, light, and motion sources with innovative wake-up mechanisms to further reduce power consumption. The ATM34/e series also features a wide harvesting input range and supports an array of storage devices, enabling smart sensors and other low-power automation applications to deliver the maximum lifespan in battery-operated devices. The SoC's radio consumes only 0.95 mA in receive and 2.5 mA in transmit at 0dB, with a programmable output power range of -20 dBm to +10 dBm, supporting low-duty-cycle operation and longer battery replacement intervals.

Mouser also offers a suite of Atmosic Technologies ATM34/e Evaluation Kits to support evaluation of the ATM34/e SoC features, energy-harvesting functionality, and performance. Atmosic's Firmware Download Board (FDL) Kit is part of a hardware and software package designed to assist in programming SoCs in production. This kit provides functionality that includes firmware, NVDS programming, and control of the Device Under Test (DUT) via the HCI interface.

The Atmosic ATMRPB reference design programming board is a connection interface adapter designed for development and debugging. This board provides a host computer access to standard development and debug interfaces on a wireless SoC-based evaluation board, or other target hardware.

The Atmosic ATM3405 tag reference design kits demonstrate the low power consumption of the Bluetooth LE device and its suitability for many applications. These design kits are based on the ATM3405 SoC, powered by a CR2032 coin cell battery and offered in a compact form factor. The ATM3405 tag reference design kits can be used as an IoT development platform by integrating external sensors or peripherals through the IoT expansion board.

To learn more, visit https://www.mouser.com/new/atmosic/atmosic-technologies-atm34-e-socs/.For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Atmosic Technologies

2026 - Atmosic™ Technologies is an innovative fabless semiconductor company, designing ultra-low power wireless and energy harvesting solutions to dramatically reduce and disrupt device dependency on batteries, aiming to deliver forever battery life and the battery-free connected Internet of Things. The company’s products enable the IoT device ecosystem—designers and manufacturers, as well as end users and those responsible for deployments—to dramatically lower costs and efforts associated with maintaining the growing Internet of Things in Personal, Home, Auto, Healthcare, Industrial, Enterprise and Smart Cities segments. In addition to these tangible business advantages, Atmosic aims to reduce ecological impacts with its vision of dramatically reducing battery consumption in the Internet of Things.


Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764