New at Mouser: AMD Alveo V80 Accelerator Card For High-Performance Compute Applications

New Product Announcement

Connect With Us


September 4, 2024Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is now shipping the Alveo™ V80 compute accelerator card from AMD. The Alveo V80 accelerator card features a powerful AMD Versal™ HBM adaptive system-on-chip (SoC) that integrates faster high-bandwidth memory (HBM2e DRAM) to overcome memory bottlenecks in high-performance compute (HPC)-applications like genomic sequencing, molecular dynamics, data analytics, network security, sensor processing, computational storage and fintech.

The AMD Alveo V80 accelerator card, available from Mouser, is based on the 7nm Versal™ adaptive SoC architecture, powered by an AMD Versal high-bandwidth memory (HBM) device, delivering 820 GB/s with 4x200G networking, PCIe® Gen4 and Gen5 interfaces, DDR4 DIMM slots for memory expansion, and Mini-Cool Edge I/O (MCIO) connectors to scale across compute and storage nodes at PCIe® Gen5 speeds. The AMD Alveo V80 accelerator is also suitable for fintech and blockchain workloads demanding massive parallelism and involving large data sets like algorithmic trading back-testing, option pricing, and Web3 blockchain cryptography.

The Alveo V80 compute accelerator card supports custom data types with the capability for 100s of nodes with built-in cryptographic engines and adaptable hardware that is also ideal for firewall and custom packet monitoring while offering the highest logic density, network throughput and memory bandwidth in the AMD Alveo portfolio.

To learn more, visit https://www.mouser.com/new/xilinx/amd-xilinx-alveo-v80-card/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, please contact:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, please contact:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764