(Source: lurii/stock.adobe.com; generated with AI)
Picture a class of nanoparticles that emit light so pure and stable they make quantum dots seem sloppy. Nanoparticles that emit light at wavelengths capable of penetrating deeply through biological tissue, including flesh and bone.
These wavelengths are so narrowly defined they sit comfortably inside the fiber-optic bands already used to shuttle vast amounts of data at near-light speed. Bands where just a few nanometers of drift make the difference between clear signal and noise.
There’s just one snag. These nanoparticles are electrical insulators, and trying to power them is like trying to fill a sealed bottle by pouring water onto it.
Seemingly impossible, right? Turns out, that’s wrong.
A team of researchers at the University of Cambridge’s Cavendish Laboratory figured out how to crack this problem[1] and get the hypothetical “water” inside the sealed bottle using lanthanide emitters, effectively powering an electrical insulator with the potential to significantly reshape medical imaging. In this blog, we trace the physics that makes lanthanide light so narrow, the reason NIR‑II travels farther through tissue than visible wavelengths, and the deceptively simple molecular bridge that turns an insulating nanoparticle into something you can actually drive like a light-emitting diode (LED).
Before we unpack the problem solved by the Cambridge team, let’s rewind a bit and talk about the nanoparticles themselves.
Lanthanides are a group of elements, such as neodymium, erbium and ytterbium, that have a rather unusual electron configuration. When you embed or “dope” their ions into a crystalline nanoparticle host, they’re able to emit that pure, stable light with all its remarkable properties.
The clarity of this light can’t be overstated. It’s the equivalent of a single voice hitting perfect pitch in a choir of different and often dissonant wavering notes. This clarity of light comes out at a highly specific narrow wavelength rather than a broad smear of colors and frequencies.
This narrow wavelength is known as the second near-infrared window, or NIR-II, and it spans roughly 1,000nm to 1,700nm.
Biological tissue is surprisingly transparent at those wavelengths. While most visible light gets scattered and absorbed within mere millimeters of entering a body, NIR-II light can penetrate 10–20mm with micrometer-scale resolution.
To put it in visual terms, it’s the difference between trying to see through fog and looking through slightly tinted glass. The difference is massive. Imagine how this might revolutionize medicine when medical professionals are able to use NIR-II to visually slice through deep tissue to see tumors, track organ function, and guide surgery without having to make any incisions.
Back to the issue of how to power these electrical insulators, however. The crystalline hosts holding the lanthanide ions have bandgaps around 8eV. For context's sake, silicon sits at about 1.1eV. At 8eV, electrons simply bounce off that bandgap like a wall. Until recently, the only way scientists could make these nanoparticles glow was to bombard them with an external light source, making it cumbersome—if not impossible—to build compact and electrically driven devices.
The Cambridge researchers found a novel way around that bandgap wall.[2] Instead of trying to force charge through an impenetrable barrier, they wrapped the nanoparticles with organic molecules that could accept electrical energy and transfer it inward by a different mechanism. This approach is like relaying a message into a soundproof room via an intermediary, rather than shouting through the walls.
Although demonstrated with lanthanides, the underlying mechanism is not material-specific.
In this case, the intermediary is a molecule called 9-anthracenecarboxylic acid (9-ACA). It's an organic dye that chemically anchors itself to the nanoparticle's surface. The molecule absorbs energy and enters what’s called a “triplet excited state.”
Typically, triplet states are considered waste. Quantum mechanical rules make them “dark,” meaning they can't release their energy as light efficiently; therefore, most optical systems treat triplet energy as lost heat.
Lanthanide ions, however, don’t play by the rules. The triplet energy transfers from the organic molecule to the lanthanide ion inside the nanoparticle with over 98 percent efficiency,[3] and it comes out as pure, narrow-wavelength NIR-II light.
The elegance of this solution is breathtaking. Like discovering that exhaust heat from your car could actually be captured and converted into electricity. The Cambridge team's solution turned discarded waste from optical systems into an entire mechanism that made impossible LEDs possible.
Even the first-generation devices resulting from this eccentric system are impressive. The LnLEDs (as the team calls them) operate at around 5V, which is somewhere within USB power territory.
They emit light with spectral linewidths as narrow as 20 nanometers, depending on the lanthanide used. For comparison, quantum dots in the near infrared typically achieve 100nm or broader. You may think that's not a huge difference at nanometer scale, but it is.
The narrower emission results in a markedly cleaner signal, meaning less interference between channels in optical communications and far better specificity for medical sensing. The current efficiency sits at around 0.6 percent,[4] which may sound modest by mature LED standards, but it's genuinely promising for devices built from materials that couldn't be electrically powered at all until now.
While the results of this novel nanoparticle solution may sound too good to be true, it's important to note that no less than two independent research teams arrived at essentially the same solution within just weeks of each other. While Cambridge was developing their approach, another collaboration of academics from Singapore, China and Hong Kong had been pursuing the same challenge for over 14 years, with Professor Liu Xiaogang of the National University of Singapore describing the early years as “chasing light trapped inside a stone.”
The breakthrough may not be limited to lanthanides alone. Scientists from the Cambridge team have noted that “countless combinations” of previously off-limit organic molecules and insulating nanomaterials are now worth exploring as electrical driving materials. The physics barrier to powering the previously un-powerable has shifted, opening up real possibilities for a brand new class of photonic devices, from wearables and denser optical networks to cutting-edge medical imaging.
The hard part was proving it could be done at all. Now it has. What needs to follow is iteration, optimization, and the slow work of turning a proof of concept into something engineers can actually build with. And that part is where all the fun and creativity resides.
For years, lanthanide nanoparticles have been a remarkable light source trapped behind an electrical wall. The moment scientists learned to move energy across that wall through molecular intermediaries, those nanoparticles stopped being laboratory curiosities and have started to look like the foundation of a whole new class of devices—poised to reshape applications such as medical imaging, optical communications, and next‑generation photonics in genuinely groundbreaking ways.
[1] ;https://www.phy.cam.ac.uk/news/tiny-antennas-to-bring-electrical-power-to-the-un-powerable-nanoparticles/ [2] https://www.nature.com/articles/s41586-025-09601-y [3] https://www.phy.cam.ac.uk/news/tiny-antennas-to-bring-electrical-power-to-the-un-powerable-nanoparticles/ [4] https://www.phy.cam.ac.uk/news/tiny-antennas-to-bring-electrical-power-to-the-un-powerable-nanoparticles/
A regular speaker on the tech conference circuit and a Senior Director at FTI Consulting, SJ Barak is an authority on the electronics space, social media in a b2b context, digital content creation and distribution. She has a passion for gadgets, electronics, and science fiction.