Estonia - Flag Estonia

Please confirm your currency selection:

Euros
Incoterms:DDP
All prices include duty and customs fees on select shipping methods.
Free shipping on most orders over 75 € (EUR).

US Dollars
Incoterms:DDP
All prices include duty and customs fees on select shipping methods.
Free shipping on most orders over $90 (USD).

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


Machine Safety Risk Assessment for Safer Industrial Automation Abhishek Jadhav

Structured risk assessment makes industrial automation fundamentally safer.

Source: Rawpixel.com/stock.adobe.com; generated with AI

Industrial automation brings both opportunity and risk. Powerful robots, conveyors, and control systems can dramatically increase productivity, but they also introduce hazards that can injure human operators or damage equipment if not properly controlled.

To manage these hazards, global and national bodies—including the International Organization for Standardization (ISO), International Electrotechnical Commission (IEC), and International Society of Automation (ISA)—provide guidelines that help engineers develop robust safety protocols. In the first part of this blog series on automation safety, we laid out critical safety standards and certifications that safeguard machines and workers operating in industrial environments. Here, we dig deeper into a core practice of every safety program: machine safety risk assessment. This is a structured method for identifying and mitigating hazards before they lead to accidents, and it is key to industrial automation delivering the efficiency required in today’s manufacturing facilities.

Advantages of a Safety Risk Assessment

Even in highly automated settings, humans still interact with machines for setup, operation, or maintenance. A formal risk assessment provides a consistent approach to identifying hazards, analyzing the risks, and defining preventive measures. The outcomes of this approach benefit several areas of automation.

Prevent Accidents and Injuries

Industrial environments, from factories to construction sites, can be hazardous, especially when large machines are in use. Therefore, a risk assessment helps predict and address potential problems. For example, detecting pinch points on a conveyor or the collision risk of a robotic arm allows teams to design safeguards, such as barriers, sensors, or access-control zones.

Minimize Downtime and Costs

Unplanned machine failures and safety incidents halt production and increase maintenance costs. A risk assessment examines where things might go wrong (e.g., a worn-out sensor that could fail, unsafe interactions between a human and a robot). By identifying potential issues before they cause breakdowns or injuries, organizations can reduce emergency stops and repairs.

Meet Regulatory and Legal Requirements

Most jurisdictions require employers to assess and mitigate workplace hazards. Performing a machine risk assessment helps organizations meet safety standards and legal obligations and provides documentation to prove compliance. In the European Union, a machine cannot be legally sold or receive a CE marking without a documented risk assessment demonstrating that all relevant safety directives have been addressed.

Protect Long-Term Operations

Regular risk assessment is an investment for the future. As technology evolves and machinery becomes more complex and automated, periodic assessment helps organizations adapt by identifying new hazards or degraded safety measures over time. This proactive approach safeguards both the workforce and the equipment.

Conducting a Machine Safety Risk Assessment

Performing a risk assessment for an industrial automation environment involves a systematic approach. Standards such as ISO 12100 (Safety of Machinery—General Principles for Design) provide a well-defined framework for this process.

Determine the Limits of the Machinery and Identify Hazards

The first step in any risk assessment is to define the machine and its use boundaries. This means describing its intended functions, operating environment, and complete life cycle, from installation and operation to maintenance and decommissioning. It also involves specifying who interacts with the equipment (e.g., operators, maintenance crews) and under what conditions.

Next, establish the different types of limits that define how the machine operates safely.

  • Use limits: what the machine is designed to do, and what constitutes misuse
  • Space limits: physical area available, including clearances, access zones, and restricted regions
  • Time limits: expected operational lifespan, maintenance intervals, or cycle times
  • Other limits: materials processed, environmental factors (such as temperature, humidity, lighting), and any special industry-specific constraints

In an automated warehouse setting, for example, defining a fleet of automated guided vehicles (AGVs) requires detailing their intended routes, load capacities, and interaction rules. Space limits would capture pedestrian exclusion zones and narrow-aisle constraints. Other limits could involve floor conditions, such as avoiding steep ramps or wet floors that increase the risk of skidding.

Once these operational boundaries are defined, engineers can systematically identify all reasonably foreseeable hazards. This part of the assessment involves examining each machine component, every operational phase, and every task performed by operators or maintenance personnel. For an AGV system, likely hazards include collision with workers or other vehicles, falling objects from storage racks, and conveyor belt entrapment.

Estimate the Risks of Each Hazard

For each identified hazard, assessors then estimate the associated risks. According to ISO 12100, risk is a combination of the severity of potential harm and the probability of its occurrence. Together, these measurements provide a risk level, which can be done qualitatively or quantitatively. Many organizations use a risk matrix or a numerical scoring system to rank risks.

A common approach is to assign a severity level (1 to 3) and a probability level (1 to 3) to the hazard. The risk might be the product of those values, or it might be a look-up table. ISO 12100 does not mandate a specific matrix, but it emphasizes considering the factors as objectively as possible.

For example, in the event of a collision between an AGV and a pedestrian, severity can range from moderate (fall injury) to high (fatality). The probability of a busy warehouse exposing pedestrians to AGVs is high, but modern sensors can help reduce the risk level. Still, such an event is possible if sensors or rules fail. The risk may be considered high, warranting reduction through better design principles.

Evaluate and Reduce Risk

Once the assessors have estimated each hazard’s risk level, they evaluate whether the risk is acceptable or if it needs to be reduced. In many cases, all but the most trivial risks will require some reduction because regulations demand a high safety standard for machinery. It is common at this stage to prioritize risks by addressing the highest risks first and ensuring critical hazards are mitigated.

Since the AGV collision example is rated as high risk, the organization would be required to implement controls such as adding safety laser scanners and traffic management software. ISO 12100 prescribes a hierarchical three-step method for risk reduction.

  1. Inherently safe design measures
  2. Safeguarding and complementary protective measures
  3. Information for use

This hierarchy reflects the principle that organizations should address hazards through design changes before resorting to guards or warnings.

Returning to the AGV collision example, the organization can address the collision hazards by redesigning the warehouse layout to minimize the number of crossing paths between humans and AGVs. The AGVs can also have a specified maximum speed limit and controlled acceleration, so even if a collision occurs, the impact is less severe. In addition, each AGV can be equipped with a 360° laser safety scanner that will slow or stop the vehicle if an obstacle is detected within a specific range.

Post-Assessment Activities

Completing the machine risk assessment and risk reduction steps is not the end of the safety process. Organizations must document the risk assessment, implement the recommended controls, verify their effectiveness, and establish a continuous safety improvement cycle.

ISO 12100 highlights that risk assessment is iterative and should be maintained throughout a machine’s life cycle. This means that even after the machine is delivered and running, the process can restart if circumstances change. For example, if a machine is moved to a new facility, the organization should perform a new review of risks. Or if a machine’s production rate increases, re-evaluate the risk levels.

By continually updating the risk assessment, organizations ensure that documentation remains current and the safety measures remain effective.

Conclusion

Risk assessment is not just a paperwork exercise, but a core engineering tool that saves lives, minimizes downtime, and ensures compliance. By adopting a structured approach of defining limits, identifying hazards, and applying the hierarchy of risk reduction measures, engineers can create and maintain safe and reliable industrial automation environments.

In the final part of this automation safety blog series, we detail the best practices for implementing functional safety, risk assessment, and protective systems in industrial automated systems.



« Back


Abhishek Jadhav received his M.S. in Electrical and Computer Engineering and started his career as a technical writer. He has over five years’ experience working as a freelance technical writer, with key interests in power electronics and embedded systems. His work has appeared in EE Times, embedded.com, and Power Electronics News, among others.


All Authors

Show More Show More
View Blogs by Date

Archives