Mouser Electronics - Electronic Components Distributor
 
Estonia - Flag Estonia

Please confirm your currency selection:

Euros
Incoterms:DDP
All prices include duty and customs fees on select shipping methods.
Free shipping on most orders over 75 € (EUR).

US Dollars
Incoterms:DDP
All prices include duty and customs fees on select shipping methods.
Free shipping on most orders over $90 (USD).

Bench Talk for Design Engineers

Bench Talk

rss

Bench Talk for Design Engineers | The Official Blog of Mouser Electronics


Bridging Bluetooth Classic and LE Audio in Embedded Systems Ezurio

How Dual-Mode Bluetooth Modules Support the Transition to LE Audio

Source: Gorodenkoff/stock.adobe.com)

Bluetooth® audio is nearly universal in modern electronic design, found in everything from industrial communications headsets to automotive infotainment and fitness equipment. What started as a simple cable replacement has become a standard part of how many devices communicate.

Developers originally built many of the deployed systems around Bluetooth Classic audio architectures. These systems were designed primarily for paired, one-to-one audio use cases. Bluetooth Classic (Basic Rate/Enhanced Data Rate) remains well-suited for these scenarios, relying on a continuous, connection-oriented link between devices, where audio streams over a dedicated channel from one source to one receiver. However, newer requirements such as synchronized audio streams, multi-stream audio, and broadcast audio are driving interest in Bluetooth LE Audio.

Emerging standards such as Bluetooth LE Audio and Auracast™ Broadcast Audio, are helping address these needs. These standards make it easier to distribute audio across multiple devices and support use cases like industrial, automotive, and public audio environments that weren't practical before.

While these new capabilities make a positive impact across applications, a new challenge arises. The existing systems aren't disappearing anytime soon. In industrial and automotive environments, especially in hardware, components can remain in service for years. Developers must design systems that support existing deployments while enabling new capabilities.

This blog explores how next-generation Bluetooth LE Audio technologies are reshaping wireless audio requirements for industrial and embedded systems, while introducing new design challenges when integrating these advancements into long-life Bluetooth Classic deployments. We discuss the limitations of legacy point-to-point architectures, outline the advantages of LE Audio, and examine how systems can be designed to bridge legacy and next-generation requirements through dual-mode solutions, enabling a practical transition without disrupting existing infrastructure.

The Migration Dilemma: Classic vs. LE Audio

Bluetooth Classic remains one of the most successful wireless standards ever developed. It's behind everything from headsets to in-vehicle hands-free systems, and in many cases, it's still the default. However, most of those systems rely on one-to-one connections, which work well for simple use cases but do not scale as systems become more complex.

At the same time, designers face increasing demands to reduce power consumption as battery-operated wireless devices run longer and become smaller and lighter—even as demand for richer audio and increased connectivity rises. Despite these pressures, Bluetooth Classic is far from obsolete. In many industrial and embedded applications, proven and stable technologies remain valuable. Nevertheless, evolving wireless audio requirements are beginning to push beyond the limits of traditional Bluetooth audio architecture.

In response, newer Bluetooth standards are introducing capabilities that address many of these limitations, although they also introduce new design considerations. Bluetooth LE Audio is one of the most significant changes to wireless audio in years. It is built on the Low Energy framework and uses isochronous channels to support synchronized unicast and broadcast audio streams across multiple devices rather than a single dedicated connection. Much of LE Audio's efficiency stems from the Low Complexity Communication Codec (LC3), which delivers high audio quality at lower bit rates than legacy Bluetooth audio codecs. In many designs, this can improve transmission efficiency and help reduce power consumption.

One of the key advancements is Auracast™ Broadcast Audio, which allows audio streams to broadcast to multiple compatible receivers simultaneously. Auracast changes how developers can distribute audio across shared environments. On a factory floor or in heavy machinery environments, broadcast audio can distribute synchronized announcements or safety instructions to entire operator teams simultaneously without relying on separate communication systems. In fitness centers, it can allow users to connect directly to shared audio streams without complex pairing procedures. This capability also applies to emergency response scenarios, where coordinated communication among multiple personnel must occur in real time.

While LE Audio and Auracast introduce attractive new capabilities, very few organizations have the luxury of replacing existing hardware infrastructure overnight. In many industries, systems remain in place for years. Industrial equipment does not get replaced quickly, and automotive timelines follow a similar pace. In addition, validated regulatory approvals and existing firmware make it difficult to change communication systems. These factors suggest that Bluetooth Classic is likely to remain active across many industries for the foreseeable future.

Meanwhile, newer products are starting to include LE Audio. As LE Audio adoption grows, new products must support these capabilities while continuing to interoperate with existing Bluetooth Classic devices. Maintaining separate hardware platforms for each standard adds complexity across development and support. Most manufacturers need existing and next-generation Bluetooth standards to coexist.

This leaves developers in a difficult situation. Trying to support both standards in one system can require redesign, but choosing just one limits what the system can connect to. As a result, designers focus much of their effort on introducing new capabilities without disrupting existing deployments.

Bridging the Gap with Dual-Mode Architecture

Tackling this type of transition calls for a way to support both legacy and next-generation audio systems within the same design without forcing a complete platform redesign.

The Ezurio Vela IF310 Multiprotocol Modules combine Bluetooth Classic (BR/EDR) support with full Bluetooth Core 6.0 Low Energy capabilities within a single wireless module. Instead of forcing developers to choose between legacy compatibility and next-generation functionality, the module allows both ecosystems to coexist within the same design. It creates a gradual migration without requiring a complete platform redesign. This approach directly addresses the reality that many teams face. Systems need to evolve without disrupting what's already in place.

Organizations can continue using legacy Bluetooth headsets while introducing Auracast-enabled broadcast communications for newer equipment. This enables incremental modernization rather than replacing entire device fleets at once.

This changes how developers can introduce new features. Instead of waiting for a full system refresh, they can layer new capabilities into existing environments as they add compatible devices over time.

Processing Power and Hardware Security

In addition to supporting legacy and next-generation wireless audio protocols, there will be a stronger emphasis on meeting the growing demand for local processing capabilities and secure data handling at the edge, as systems become more connected and distributed. Meeting these requirements depends on how much processing and control can be handled directly within the wireless module.

The Ezurio Vela IF310 module also provides substantial integration flexibility. A 192 MHz Arm® Cortex®-M33 processor supports both hosted and hostless architectures, enabling developers to tailor system designs according to application requirements. The module can operate alongside an external host processor or consolidate processing directly onto the module to reduce board complexity, bill of materials (BOM) cost, and firmware overhead. This flexibility particularly benefits embedded designs, where designers must carefully manage space, power, and system complexity.

Alongside processing considerations, systems must increasingly handle data securely, especially as wireless audio streams may carry sensitive information that requires protection without compromising performance. The Vela IF310 incorporates hardware-level security technologies, including TrustZone® and CryptoCell-312. By handling security functions at the hardware level, the module can support secure communication while minimizing the latency and timing disruptions that can impact real-time audio performance. Together, these capabilities position the module as a practical migration platform for long-life embedded systems.

Conclusion

Technologies such as LC3 and Auracast are expanding the capabilities of wireless audio systems, enabling more flexible communication solutions for industrial, automotive, and commercial applications.

Bluetooth Classic infrastructure is unlikely to disappear soon, and many deployed systems will stay in place for years. The challenge for developers is adding newer LE Audio capabilities without forcing a full redesign.

Dual-mode platforms such as the Ezurio Vela IF310 help address the transition. By supporting both Bluetooth Classic and LE Audio in a single module, they let developers add new features while continuing to work with existing devices. This reduces the need to choose between maintaining legacy compatibility and supporting newer standards, while also minimizing redesign, limiting integration risk, and shortening the path to deployment for updated systems.

Author

David Pike is well known across the interconnect industry for his passion and general geekiness. His online name is Connector Geek.



« Back


Ezurio turns design possibility into reality with a comprehensive range of RF modules, system-on-modules, single board computers, internal antennas, IoT devices, and custom solutions. With decades of engineering expertise, Ezurio provides solutions that reduce development costs and time to market. Ezurio's global reach and unmatched support are backed by a resilient global supply chain that gives our customers the stability to overcome every design challenge with confidence. Turn design possibility into reality with Ezurio, your connectivity expert.


All Authors

Show More Show More
View Blogs by Date

Archives